When working with the mmwave_sdk_68xx_aop_hwa/main.c code in Code Composer Studio, I keep getting the pictured error when attempting to "build project". This is without making any changes to the demo code. Is this error a problem? We would like to make changes to the demo code and have it compile so that we can flash it to the board, however the concern is that if we receive this error even without changing anything at all we may not be able to compile the code after we make changes. Is this error preventing compilation of the code or can it be rightfully ignored?