This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP411-Q1: What's the difference between TMP411-Q1 and TMP411ADGKR

Part Number: TMP411-Q1
Other Parts Discussed in Thread: TMP411

Hi team,

What's the difference between TMP411-Q1 and TMP411ADGKR

1. Can pin to pin be replaced directly without changing the layout?

2. What is the difference between the two? Does customer need to change the software to replace it?

  • Hi Jason,

    The TMP411-Q1 is AEC-Q100 qualified and has slightly different ESD ratings from the TMP411. The customer will not need to make layout or software changes, because both devices will meet the same electrical specifications and are pin-to-pin compatible.

    Best regards,
    Nicole