This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: Custom board considerations

Part Number: MMWCAS-DSP-EVM

Hi,

we are developing a custom board based in the MMWCAS-DSP-EVM (tda2xx), and we want to include the DCAN1 interface (connected to a transceiver). From the MMWCAS-DSP-EVM's schematics we have seen that this pins are connected to two signals (TDA_GPIO1_15_ALERT# and TDA_GPIO1_14_FPGA_FLASH_RESETn). From the code (Processor_SDK_Radar), both GPIOs (GPIO1_14 and GPIO1_15) dont seem to be used (this is our impression). Could you confirm us if there is a functionality of these GPIOs in the software part?

We want to make sure if it is necessary remap these signal to other free pads or can get rid of them.

Thank you!!