I am using IWR1642BOOST. I checked that if in the guiMonitor (-1 1 1 1 1 1 1), I enable all the tlv_types as listed below my frame rate becomes 4FPS.
- Detected Points
- Range Profile
- Noise Profile
- Azimuth Static Heatmap
- Range-Doppler Heatmap
- Statistics
I want to increase this frame rate. If I increase it manually in the framecfg (0 1 16 0 10 1 0) there is no USB output. It only outputs when the frame rate is 4FPS i.e. framecfg (0 1 16 0 250 1 0).
For my particular application, I need a range of up to 2 meters. Can I drop the redundant range bins and increase my frame rate??