This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843LEVM: Some issues with the python gui exe

Part Number: IWR6843LEVM


Hi team,

Customer has a question:

I am trying out of box demo for iwr6843levm.

I am able to run the demo on the online mmwave demo visualiser.

However, when i try it on the mmwave people counting gui downloaded. The images remian stagnant:

After which it does not respond. The console have the following error message:

The configuration used:

% ***************************************************************
% Created for SDK ver:03.06
% Created using Visualizer ver:3.6.0.0
% Frequency:60
% Platform:xWR68xx
% Scene Classifier:best_range_res
% Azimuth Resolution(deg):15 + Elevation
% Range Resolution(m):0.043
% Maximum unambiguous Range(m):17.61
% Maximum Radial Velocity(m/s):1
% Radial velocity resolution(m/s):0.13
% Frame Duration(msec):100
% RF calibration data:None
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% Angle of Arrival FoV: Full FoV
% Range FoV: Full FoV
% Doppler FoV: Full FoV
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 60 349 7 66.67 0 0 60 1 496 8454 0 0 158
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
frameCfg 0 2 16 0 100 1 0
lowPower 0 0
guiMonitor -1 1 1 0 0 0 1
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 6 121 0
CQSigImgMonitor 0 123 8
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 16.90
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart
May I know how can i resolved it? I am using windows 10.

Thanks

Best regards

Jiahui

  • Hello Jiahui.

    I wasn't able to replicate your issue with the people counting visualizer and your configuration settings.  However, I found another bug in your profileCfg where you ended up having too many adc samples as it has to be below 256.  In addition, when the ramp end time is reduced to below 66, I was able to get it working with the people counting visualizer.

    Sincerely,

    Santosh