This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900: PGA900 GUI on Win10

Genius 17335 points
Part Number: PGA900

Hello,

I installed PGA900 GUI software along with labview runtime 2012 on my PC (Windows 10 Pro, 21H2).
When I tried to launch the PGA900 GUI sotware, it showed the below error message.

Sorry, it is Japanese, but it says

Labview runtime engine can't be found.
PGA900 requires version 2012(or compatible version) of Labview runtime eingine.
To solve this probelm, you need to contact to the PGA900 developer or dowonload Labview runtime engine from national insturments web site.
Do you download the LabVIEW runtime eingeen by accessing ni.com?

Yes : No : Cancel.


I have dowonloaded and installed 2012 version ( I also tried 2012 SP1) of Labview runtime engine. 
But this error still was showed after installing the runtime.

Does PGA900 GUI run on Win10?

Regards,
Oba