I am a design engineer creating a 1-Layer ceramic substrate to support the HD3022 humidity sensor. The data sheet calls for a 0.1µF bypass cap to be placed between VDD and GND pins #5 and #8. One option (most simple based on my design constraints) is to rout the ADDR1 and RESET pin traces beneath the HDC3022 sensor and out to the edge of the ceramic carrier. I can then bridge VDD and GND traces with the cap without risk of shorting to ADDR1 or RESET.
This however means the thermal pad beneath the humidity sensor will be in contact with the ADDR1 and RESET traces during measurement.
Is this a problem from an electrical perspective?