Other Parts Discussed in Thread: UNIFLASH
Good morning,
1. I have configured the mmWave Sensor IWR6843AOPEVM with mmWaveDemoVisualizer but don't get any data after switching to a microcontroller, which shall read the data. I have the assumption that the mmWaveDemoVisualizer configures the sensor only temporarily and the configuration gets lost after power-off of the sensor. Is that the case?
2. How do I configure the sensor correctly and permanently? I have found an example file to use with Uniflash, but the COM does not connect (I double checked that it is the right COM) and the sensor is being found when using mmWave Sensor.
3. If (2) is the way to go: How do I set parameters in such a file alike the parameters I can set in mmWaveDemoVisualizer? How do I make such a file?
Note: I do not have any additional hardware such as DCA1000. Do I need it for this?
Thank you very much in advance!
Sincerely
Marius von Wisotzky