This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: VBGAP and VOUT_14APLL

Part Number: IWR6843
Other Parts Discussed in Thread: UNIFLASH

Dear support team,

We have designed original antenna board with IWR6843.

It is succeeded to write firmware by uniflash but to boot up is failed and no UART communication is observed.

Then, we are debugging the board by following "HW bringup guidelines" in attached file, and we notice VBGAP voltage is 0.73V, which is 18% down to 0.9V.

Also, VOUT_14APLL ivoltage s 1.12V, which is also 18% down to 1.4V. I suppose the voltage drop may be critical for booting up.

We would like to know which pins are related to generate VBGAP voltage and VOUT_14APLL voltage.

Also, we are fine if we could get internal voltage subsystem to understand how to generate VBGAP and VOUT_14APLL for IWR6843.

Best regards,

Taka4064.HardwareDesignChecklist_V0p8_IWR6843.xlsx