This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC3020: Pin-to-pin/drop in with SHT30?

Part Number: HDC3020

Hi,

I checked the pinout of the HDC3020 and the SHT30 from Sensirion and they look pin-to-pin compatible (with maybe the exception of pin 7 being ADDR1 vs R), but I was wondering if this part would be drop-in? If not, what modifications would be needed?

Also the only orderable for this part is PHDC3020DEFT, this is due to the part being in pre-production correct?

Thank you!

  • Hello,

    The SHT30 and the HDC3020 are pin-2-pin compatible. You won't need any further modifications as long as the component has the required bypass cap and the pull up resistors. 

    Currently only the PHDC3020DEFT is available as the device isn't released yet. We plan on releasing the IC later this month.

    Regards,
    Pavani Tenneti