This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: max object speed

Part Number: IWR6843ISK

If there is a flat object of with cross section diameter of 0.5m, moving directly away from the antenna, is there a formula to calculate the maximum speed the IWR6843ISK can detect the object moving away? For example, could it detect the object moving away at 100 meters per second?