Is there any streaming lua script which I can use as a reference for streaming mode?
Kia
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there any streaming lua script which I can use as a reference for streaming mode?
Kia
Well I see the following modes included in the lua script I am using, I assume "streaming mode" means continuous, non-stop frame transmission or something similar. Is this a correct understanding?
--Legacy Framing mode = 0/Advanced framing mode = 1/Continuous streaming mode = 2
Hi Cesar,
We are planning to run a continuous raw data capture on the PC using our DCA1000 capture board. Does mmWave Studio support this operation? If so, can you share a lua or any type of script which we can try? If not, what could be the best alternative solution?
Your prompt response is highly appreciated.
Kia
Hi,
Sorry for the delay
With DCA1000 it is possible to capture raw data to a file. It is not possible to perform continuous raw data streaming.
We don't have a solution for continuous raw data streaming.
Thank you
Cesar
Just making sure, it is not possible with DCA1000 to perform continuous raw data streaming on mmWave Studio or can it be performed on other platforms such as dfp code by making changes in its source codes? I am able to have continuous streaming but has 2 seconds delay between each capture both with mmWave Studio and dfp.
Thanks again
Kia
Hi,
No, we don't have any platform where one could stream raw data.
Thank you
Cesar