This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: AWR1843 - Create CCS project for Demo/xwr18xx/mmw but sysbios tasks could not task because of exception

Part Number: AWR1843BOOST

Hi team, 

I have created a CCS version 11.2 project for mmwave_sdk_03_06_00_00-LTS\packages\ti\demo\xwr18xx\mmw. I have added all the necessary libraries into both mss/dss projects then built successfully. 

However, flash the binary file into awr1843boost, but the sensor could not run properly. I figured out that MSS tasks could not launched but fall into exception. I am not sure if any things missed when created CCS project, I kept the source code as same as demo source code.

I was able to compile and run ok with the same demo source on command line environment, was motivated to create a CCS project to make use of the GUI debug features. 

Please find more details in the attachments

**** Build of configuration Debug for project awr18xx_mmw_dss ****

"C:\\ti\\ccs1120\\ccs\\utils\\bin\\gmake" -k -j 8 all -O 
 
Building file: "../mmw_dss.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_50_08_24_core/xs" --xdcpath="C:/ti/dsplib_c64Px_3_4_0_0/packages;C:/ti/dsplib_c674x_3_4_0_0/packages;C:/ti/mathlib_c674x_3_1_2_1/packages;C:/ti/bios_6_73_01_01/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C674 -p ti.platforms.c6x:AWR18XX:false:600 -r release -c "C:/ti/ti-cgt-c6000_8.3.3" "../mmw_dss.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring mmw_dss.xe674 from package/cfg/mmw_dss_pe674.cfg ...
generating custom ti.sysbios library makefile ... 
Starting build of library sources ...
making C:/awr18xxFW/awr18xx_mmw_dss/src/sysbios/sysbios.ae674 ...
gmake[1]: Entering directory `C:/awr18xxFW/awr18xx_mmw_dss/src/sysbios'
gmake[1]: Nothing to be done for `all'.
gmake[1]: Leaving directory `C:/awr18xxFW/awr18xx_mmw_dss/src/sysbios'
Build of libraries done.
cle674 package/cfg/mmw_dss_pe674.c ...
Finished building: "../mmw_dss.cfg"
 
Building file: "../antenna_geometry.c"
Invoking: C6000 Compiler
"C:/ti/ti-cgt-c6000_8.3.3/bin/cl6x" -mv6740 --abi=eabi -O0 --include_path="C:/awr18xxFW/awr18xx_mmw_dss" --include_path="C:/ti/ti-cgt-c6000_8.3.3/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --define=SOC_XWR18XX --define=NO_ANTENNA_CORRECTION --define=SUBSYS_DSS --define=APP_RESOURCE_FILE="<mmw_res.h>" --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_L3RAM_SIZE=0x100000 --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="antenna_geometry.d_raw" --cmd_file="configPkg/compiler.opt"  "../antenna_geometry.c"
Finished building: "../antenna_geometry.c"
 
Building file: "../data_path.c"
Invoking: C6000 Compiler
"C:/ti/ti-cgt-c6000_8.3.3/bin/cl6x" -mv6740 --abi=eabi -O0 --include_path="C:/awr18xxFW/awr18xx_mmw_dss" --include_path="C:/ti/ti-cgt-c6000_8.3.3/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --define=SOC_XWR18XX --define=NO_ANTENNA_CORRECTION --define=SUBSYS_DSS --define=APP_RESOURCE_FILE="<mmw_res.h>" --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_L3RAM_SIZE=0x100000 --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="data_path.d_raw" --cmd_file="configPkg/compiler.opt"  "../data_path.c"
Finished building: "../data_path.c"
 
Building file: "../dss_main.c"
Invoking: C6000 Compiler
"C:/ti/ti-cgt-c6000_8.3.3/bin/cl6x" -mv6740 --abi=eabi -O0 --include_path="C:/awr18xxFW/awr18xx_mmw_dss" --include_path="C:/ti/ti-cgt-c6000_8.3.3/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --define=SOC_XWR18XX --define=NO_ANTENNA_CORRECTION --define=SUBSYS_DSS --define=APP_RESOURCE_FILE="<mmw_res.h>" --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_L3RAM_SIZE=0x100000 --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="dss_main.d_raw" --cmd_file="configPkg/compiler.opt"  "../dss_main.c"
Finished building: "../dss_main.c"
 
Building file: "../objectdetection.c"
Invoking: C6000 Compiler
"C:/ti/ti-cgt-c6000_8.3.3/bin/cl6x" -mv6740 --abi=eabi -O0 --include_path="C:/awr18xxFW/awr18xx_mmw_dss" --include_path="C:/ti/ti-cgt-c6000_8.3.3/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --include_path="C:/ti/mathlib_c674x_3_1_2_1/packages" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft16x16/c64P" --include_path="C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/src/DSP_fft32x32/c64P" --define=SOC_XWR18XX --define=NO_ANTENNA_CORRECTION --define=SUBSYS_DSS --define=APP_RESOURCE_FILE="<mmw_res.h>" --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_L3RAM_SIZE=0x100000 --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --preproc_with_compile --preproc_dependency="objectdetection.d_raw" --cmd_file="configPkg/compiler.opt"  "../objectdetection.c"
Finished building: "../objectdetection.c"
 
Building target: "awr18xx_mmw_dss.xe674"
Invoking: C6000 Linker
"C:/ti/ti-cgt-c6000_8.3.3/bin/cl6x" -mv6740 --abi=eabi -O0 --define=SOC_XWR18XX --define=NO_ANTENNA_CORRECTION --define=SUBSYS_DSS --define=APP_RESOURCE_FILE="<mmw_res.h>" --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_L3RAM_SIZE=0x100000 --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number -z -m"awr18xx_mmw_dss.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ti-cgt-c6000_8.3.3/lib" -i"C:/ti/ti-cgt-c6000_8.3.3/include" -i"C:/awr18xxFW/awr18xx_mmw_dss" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/control/mmwave/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/control/mmwavelink/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/control/dpm/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/datapath/dpc/dpu/aoaproc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/datapath/dpc/dpu/cfarcaproc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/datapath/dpc/dpu/dopplerproc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/datapath/dpc/dpu/staticclutterproc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/datapath/dpedma/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/datapath/dpu/rangeproc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/crc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/mailbox/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/osal/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/soc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/uart/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/edma/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/adcbuf/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/alg/mmwavelib/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/hwa/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/utils/mathutils/lib" -i"C:/ti/dsplib_c64Px_3_4_0_0/packages/ti/dsplib/lib" -i"C:/ti/mathlib_c674x_3_1_2_1/packages/ti/mathlib/lib" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="awr18xx_mmw_dss_linkInfo.xml" --rom_model -o "awr18xx_mmw_dss.xe674" "./antenna_geometry.obj" "./data_path.obj" "./dss_main.obj" "./objectdetection.obj" "../c674x_linker.cmd" "../mmw_dss_linker.cmd" -l"configPkg/linker.cmd"  -llibc.a -llibosal_xwr18xx.ae674 -llibsoc_xwr18xx.ae674 -llibcrc_xwr18xx.ae674 -llibuart_xwr18xx.ae674 -llibmailbox_xwr18xx.ae674 -llibmmwavelink_xwr18xx.ae674 -llibmmwave_xwr18xx.ae674 -lmathlib.ae674 -ldsplib.ae64P -llibedma_xwr18xx.ae674 -llibadcbuf_xwr18xx.ae674 -llibmmwavealg_xwr18xx.ae674 -llibhwa_xwr18xx.ae674 -llibdpm_xwr18xx.ae674 -llibaoaproc_hwa_xwr18xx.ae674 -llibcfarcaproc_hwa_xwr18xx.ae674 -llibdopplerproc_hwa_xwr18xx.ae674 -llibstaticclutterproc_xwr18xx.ae674 -llibrangeproc_hwa_xwr18xx.ae674 -llibdpedma_hwa_xwr18xx.ae674 -llibmathutils.ae674 -lrts6740_elf.lib 
<Linking>
Finished building target: "awr18xx_mmw_dss.xe674"
 
C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/scripts/ImageCreator/out2rprc/out2rprc.exe awr18xx_mmw_dss.xe674 awr18xx_mmw_dss.bin
Parsing the input object file, awr18xx_mmw_dss.xe674.
Appending zeros 8487936
Appending zeros 8514736
File conversion complete!
 

**** Build Finished ****
.
**** Build of configuration Debug for project awr18xx_mmw_mss ****

"C:\\ti\\ccs1120\\ccs\\utils\\bin\\gmake" -k -j 8 all -O 
 
Building file: "../mmw_mss.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_50_08_24_core/xs" --xdcpath="C:/ti/dsplib_c64Px_3_4_0_0/packages;C:/ti/dsplib_c674x_3_4_0_0/packages;C:/ti/mathlib_c674x_3_1_2_1/packages;C:/ti/bios_6_73_01_01/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.R4F -p ti.platforms.cortexR:AWR18XX:false:200 -r release -c "C:/ti/ti-cgt-arm_16.9.6.LTS" "../mmw_mss.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring mmw_mss.xer4f from package/cfg/mmw_mss_per4f.cfg ...
generating custom ti.sysbios library makefile ... 
Starting build of library sources ...
making C:/awr18xxFW/awr18xx_mmw_mss/src/sysbios/sysbios.aer4f ...
gmake[1]: Entering directory `C:/awr18xxFW/awr18xx_mmw_mss/src/sysbios'
gmake[1]: Nothing to be done for `all'.
gmake[1]: Leaving directory `C:/awr18xxFW/awr18xx_mmw_mss/src/sysbios'
Build of libraries done.
cler4f package/cfg/mmw_mss_per4f.c ...
Finished building: "../mmw_mss.cfg"
 
Building file: "../mmwdemo_adcconfig.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mmwdemo_adcconfig.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_adcconfig.c"
Finished building: "../mmwdemo_adcconfig.c"
 
Building file: "../mmwdemo_flash.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mmwdemo_flash.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_flash.c"
Finished building: "../mmwdemo_flash.c"
 
Building file: "../mmwdemo_monitor.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mmwdemo_monitor.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_monitor.c"
Finished building: "../mmwdemo_monitor.c"
 
Building file: "../mmwdemo_rfparser.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mmwdemo_rfparser.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_rfparser.c"
Finished building: "../mmwdemo_rfparser.c"
 
Building file: "../mmw_lvds_stream.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mmw_lvds_stream.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmw_lvds_stream.c"
Finished building: "../mmw_lvds_stream.c"
 
Building file: "../mmw_cli.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mmw_cli.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmw_cli.c"
Finished building: "../mmw_cli.c"
 
Building file: "../mss_main.c"
Invoking: Arm Compiler
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --include_path="C:/awr18xxFW/awr18xx_mmw_mss" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS" --include_path="C:/ti/mmwave_sdk_03_06_00_00-LTS/packages" --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi --preproc_with_compile --preproc_dependency="mss_main.d_raw" --cmd_file="configPkg/compiler.opt"  "../mss_main.c"
Finished building: "../mss_main.c"
 
Building target: "awr18xx_mmw_mss.xer4f"
Invoking: Arm Linker
"C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me --define=_LITTLE_ENDIAN --define=MMWAVE_L3RAM_NUM_BANK=8 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=SHMEM_ALLOC=0x00000008 --define=DebugP_ASSERT_ENABLED -g --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --abi=eabi -z -m"awr18xx_mmw_mss.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ti-cgt-arm_16.9.6.LTS/lib" -i"C:/ti/ti-cgt-arm_16.9.6.LTS/include" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/control/mmwave/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/control/mmwavelink/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/crc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/esm/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/gpio/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/osal/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/pinmux/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/mailbox/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/dma/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/soc/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/uart/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/canfd/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/adcbuf/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/cbuff/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/csi/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/edma/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/control/dpm/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/qspi/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/drivers/qspiflash/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/utils/mathutils/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/utils/hsiheader/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/utils/cli/lib" -i"C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/ti/utils/rtrim/lib" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="awr18xx_mmw_mss_linkInfo.xml" --rom_model -o "awr18xx_mmw_mss.xer4f" "./mmw_cli.obj" "./mmw_lvds_stream.obj" "./mmwdemo_adcconfig.obj" "./mmwdemo_flash.obj" "./mmwdemo_monitor.obj" "./mmwdemo_rfparser.obj" "./mss_main.obj" "../mmw_mss_linker.cmd" "../r4f_linker.cmd" -l"configPkg/linker.cmd"  -llibc.a -llibosal_xwr18xx.aer4f -llibesm_xwr18xx.aer4f -llibgpio_xwr18xx.aer4f -llibsoc_xwr18xx.aer4f -llibmailbox_xwr18xx.aer4f -llibpinmux_xwr18xx.aer4f -llibcrc_xwr18xx.aer4f -llibDMA_xwr18xx.aer4f -llibuart_xwr18xx.aer4f -llibcanfd_xwr18xx.aer4f -llibmmwavelink_xwr18xx.aer4f -llibmmwave_xwr18xx.aer4f -llibcli_xwr18xx.aer4f -llibadcbuf_xwr18xx.aer4f -llibcbuff_xwr18xx.aer4f -llibedma_xwr18xx.aer4f -llibdpm_xwr18xx.aer4f -llibqspiflash_xwr18xx.aer4f -llibqspi_xwr18xx.aer4f -llibmathutils.aer4f -llibhsiheader_xwr18xx.aer4f -lrtsv7R4_T_le_v3D16_eabi.lib -llibrtrimutils.aer4f 
<Linking>
warning #16027-D: object files have incompatible enumeration types ("C:\hoplo_ws\HoploFW\awr18xx_mmw_mss\Debug\configPkg\package\cfg\mmw_mss_per4f.oer4f" = packed, "./mmw_cli.obj" = 32-bit)
Finished building target: "awr18xx_mmw_mss.xer4f"
 
C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/scripts/ImageCreator/out2rprc/out2rprc.exe awr18xx_mmw_mss.xer4f awr18xx_mmw_mss.bin
Parsing the input object file, awr18xx_mmw_mss.xer4f.
Appending zeros 0
Appending zeros 256
Appending zeros 143832
File conversion complete!
C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/scripts/ImageCreator/multicore_image_generator/MulticoreImageGen.exe LE 37 0x00000008 mmw_awr18xx.bin 0x35510000 C:/awr18xxFW/awr18xx_mmw_mss/Debug/awr18xx_mmw_mss.bin 0xb5510000 C:/ti/mmwave_sdk_03_06_00_00-LTS/firmware/radarss/xwr18xx_radarss_rprc.bin 0xd5510000 C:/awr18xxFW/awr18xx_mmw_dss/Debug/awr18xx_mmw_dss.bin
Number of Input Files 3
Number of zeros 24
Number of zeros 8
 
C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/scripts/ImageCreator/crc_multicore_image/crc_multicore_image.exe mmw_awr18xx.bin mmw_awr18xx.bin.tmp
size of App Image is 345088 bytes
cur_crc_read_addr 128
cur_crc_read_addr 148736
cur_crc_read_addr 183616
Failed to remove CRC temp file
 
C:/ti/mmwave_sdk_03_06_00_00-LTS/packages/scripts/ImageCreator/append_bin_crc/gen_bincrc32.exe mmw_awr18xx.bin
>>>> Binary CRC32 = 1b4f46ae <<<<
>>>> Total bytes in binary file 345092 <<<<
 
 

**** Build Finished ****

Appreciate your help to figure the issues. 

Thanks, 

QL