Hi,
1.I am working on mmwaveSDK 3.5, IWR6843ISK board and trying to extract and store Doppler FFT out in L3 memory for the doppplerprocDPU.
I have changed the pipeline slightly where i chained the DetMatrix EDMA configuration with the newly configured 2dFFT output EDMA configuration, instead of EDMA In(Radarcube to HWA memory for 2dFFT).
Also I have chained 2dFFT output EDMA configuration with the EDMA In.
which looks like this-
|-------DummyHWA-------EDMA_new_out
|
Radarcube-------EDMAIn------HWA(dopplerFFT+log)-------HWA(Sum of Magnitude) HWA(Dummy for storing doppler fft)-------EDMAout
I have configured a dummy HWA after Sum of Magnitude HWA, which EDMAouts the DopplerFFT data to L3.
The problem that i am facing while comparing the default pipeline DetMatrix output with my implemented
pipeline DetMatrix output is that its is matching for only 512 bytes(1 ping 1 pong) out of 8KB.
2. I want to store raw adc data for a few frames in L3 memory in the same pipeline, without disturbing the pipeline, without using the DVA1000EVM. Is it possible, how do i go ahead with it ?
Please help me resolve the issues.
Thankyou