This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: AWR1843BOOST How to write millimeter wave radar settings

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843

How can I change the radar parameters directly without using the demo provided in AWR1843BOOST?

  • Hi yousuke nasu,
    So the AWR1843 is autonomous sensor, in which user can write their own application for configuring the front end of the device.
    We have provided the mmwavelink library, so that the user can call the API's (present in the library) in the application which will configure the front-end.
    If you want reference to how it is configured you can also refer the following below which utilizes the mmwavelink library for configuration - 
    C:\ti\mmwave_sdk_03_05_00_04\packages\ti\control\mmwavelink\test

    The frame and chirp configurations are general radar parameters. If you are looking at some other specific parameter, do reply to this thread.
    Hope resolves your queries.
    Regards,
    Saswat Kumar