Other Parts Discussed in Thread: UNIFLASH
I don’t know why sometimes it shows connected sometimes it shows one out of two connected and sometimes it shows two out of two connected,
The recent one is two out of two connected. I don’t know why this is happening. I am using the correct power 5 V 2. 5 A,
i’m using USB cable for UART, do I need to change the IP address manually? Like 192 168 33 30?If so how do I do it in Linux? I can only use Linux..
I already flashed demo bin using uniflash I am using mmwave SDK 3.2.4,
comforts are also correct,
When I use MM wave demo visualizer, do I need to set my board on 001 (SOP mode 4) = functional mode? By the way is 001 mean SOP2 is 1 or SOP0 is 1?