This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Inquiries for Radar Applicable Area

Part Number: IWR6843ISK

Hi TI Champs.

Can you checm if the following application area would be applicable with IWR6843ISK sensros?

If you need multiple sensors, please recommend the number of sensors.

Implementation Features

Range

Number of people detected

Heart rate and respiratory rate sensing

1~2m

14 people

Fall sensing

50cm

20 people

Moving Overhead and Speed Sensing

30m

14 people

Thanks.
Regards, 
Jack