Hi Experts,
Good day. Seeking your advise on this query I posted on behalf of my Cx:
I am facing the following problem while trying to measure the coordinates of my target (trihedral corner reflector) using AWR1843BOOST. I am using the mmwave Demo visualizer.
1. I tried calibrating using the compRangeBiasAndRxChanPhase
As mentioned in the file- C:\ti\mmwave_sdk_03_06_00_00-LTS\packages\ti\demo\xwr18xx\mmw\docs\doxygen\html\index.HTML for the
While this seems to improve the error in the Z-axis, I am getting incorrect values in the Y-axis direction.
2. Also, when I increase the distance of the target beyond the range resolution, I start getting incorrect coordinates for all three (x,y,z).
3. Suppose my range resolution is 0.341 m for bandwidth 77GHz, as soon as I keep my target at 0.35 m (or any a few cms far from 0.341 m) the range shown in the plot becomes 0.682 (twice it)
Can you suggest what might be the issue? I am using only the AWR1843BOOST board along with the mmw_demo_example_script file.
What other things i should do to increase the accuracy of the x,y, and z coordinates for my data? Either in physical placement or configuration etc.
PN: AWR1843BOOST
Thank you.
Regards,
Archie A.