This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: 68xx vital signs

Part Number: IWR6843ISK

Hi,

After the customer burns vital_signs.bin, the following content appears after running VitalSignsRadar_Demo.exe, and there is no data output in the GUI:

QT version = 5.9.1
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
Serial Port Found
Data Port Number is "COM9"
User Port Number is "COM10"
Data port succesfully Open
User port succesfully Open
Configuration File Name Read from the GUI is %s/n "xwr1642_profile_VitalSigns_20fps_Back.cfg"
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
"COM10"
Configuration File Path is %s/n "D:/mmwaveSDK/ccs1200/mmwave_industrial_toolbox_4_12_0/labs/Vital_Signs/68xx_vital_signs/gui/profiles/xwr1642_profile_VitalSigns_20fps_Front.cfg"
Chirp Duration in us is : inf
Chirp Bandwidth in kHz is : inf
Maximum Range in Meters is : nan
Range-FFT size is : 32768
Range-Bin size is : nan
Range-Bin Start Index is : -2147483648
Range-Bin End Index is : -2147483648
Total Payload size from the UART is : 188
Padding Factor is : 6
Total Payload size from the UART is : 192

  • Hi Nancy,

    This GUI is known to have issues related to the GUI. The customer should start by evaluating the Vital Signs with People Tracking lab, if possible. 

    I am sorry I cannot be more helpful, but this is a legacy lab. The customer is welcome to debug the gui source code located at mmw_industrial_toolbox\labs\Vital_Signs\68xx_vital_signs\gui\gui_source

    Thank you,

    Angie