Other Parts Discussed in Thread: AWR1843AOP
Hello,at first I wanted to use IWR6843AOP to use gesture recognition demo.Unfortunately,only the last step, can not show the results.
So,I intend to run out of bow demo to verify that the board output is normal.Now,the CFG port can be connected,but the data port is not.

I have noticed the SDK version and mmWave Demo Visualizer version. SDK is 03.05.00.04;mmWave Demo Visualizer is 3.5.0.SDK is 03.06.00.00;mmWave Demo Visualizer is 3.6.0.
The 6843AOP image in SDK 3.5 and SDK 3.6 and industrial tool box 4.10.0 have been tried.But the data port is not connected.
In order to verify whether there is a problem with the computer equipment, it is found that the connection to AWR1843AOP is not this problem, and the same data line is selected.

I also noticed that the working mode is switched, and the operation should be fine.

Is IWR6843AOP data port broken?But someone has successfully run the out of box demo with IWR6843AOP before.