Other Parts Discussed in Thread: IWR6843AOPEVM, IWR1843BOOST
Hi,
Currently i have IWR1443BOOST EVM module.
I checked this link "dev.ti.com/.../node (radar ros-driver) to get the Pointcloud.
I got to know my module is a bit older and i am in process to purchase few other new module.
Please clarify my few doubts-
1) Does any of these IWR1843BOOST / IWR6843AOPEVM or any radar give the reflectivity as output in ROS? From above link, it says the output pointcloud is based on intensity. Does this mean reflectivity also?
2) i want to build a 2D/3D map from the pointcloud of radar so I am considering if that pointcloud is made up of material reflectivity, then i can interpret each reflective point to identify the material such as wood, metal etc.
If any of the radar does that , i would love to order that.
Thanks.