This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: computer is not recognizing the device, no com ports emulated

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR6843AOP

I recently received the IWR6843AOPEVM mmWave sensor eval kit. 

I am unable to begin testing with this kit as my computer is not recognizing the device... no com ports are emulated.

The ports aren’t shown correctly.
I  installed the driver but that didn’t work.
  • Hi Matthew,

    Couple of questions for you:

    1. You mentioned you are using the IWR6843AOP, are you using this device standalone or with the MMWAVE-ICBOOST carrier board?
    2. If using the device standalone, can you please confirm which USB port you are connected to on the EVM? It should be USB1.
    3. Which drivers did you install? There are different drivers needed for standalone EVM compared to EVM+ICBOOST.

    Best Regards,

    Josh