This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV5023-Q1: Minimum Distance to capacitor

Part Number: DRV5023-Q1


My customer has a layout using 2x DRV5023BIEDBZRQ1. One is very close to a large capacitor. 

the Hall sensor has a distance of 1.3mm from the plastic bracket of capacitor, 2mm from the capacitor aluminum body.Could you please check if this placement will affect the Hall sensor? or can recommended the minimum distance from the capacitor?

Capacitor is UUE1V101: https://www.nichicon.co.jp/english/products/pdfs/e-uux.pdf 

Thanks!

  • Hello ReedKacz,

    I do not think that capacitor should have much impact on your hall sensor measurement.  Typically we expect magnetic flux to be diverted and concentrated into highly permeable materials, which would be the path of least reluctance (magnetic resistance).  Highly permeable materials would include Iron, Nickel, and cobalt.  Aluminum and copper have a relative permeability similar to air.