This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Debugging issues after importing vitalSigns example project

Part Number: IWR6843

Hii TI Technical Forum team,

 We are using mmwave SDK version: mmwave_sdk_03_01_01_02 , CCS version: v12, mmwave_industrial_toolbox_3_2_0.

while doing the debugging the following error messages are encountered.

we are wondering if the issue is related to the version of CCS? if so it would be through it if u can point us towards the technical notes on the CCS version vs mmwave SDK.

Building file: "../vitalSigns.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_50_04_43_core/xs" --xdcpath="C:/ti/bios_6_73_01_01/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.R4F -p ti.platforms.cortexR:IWR14XX:false:200 -r release -c "C:/ti/ti-cgt-arm_16.9.6.LTS" "../vitalSigns.cfg"
subdir_rules.mk:19: recipe for target 'build-1803236881-inproc' failed
C:\ti\xdctools_3_50_04_43_core\C:/ti/xdctools_3_50_04_43_core/xs: error: can't create session manager: create of JVM failed
gmake[2]: *** [build-1803236881-inproc] Error 1
subdir_rules.mk:16: recipe for target 'build-1803236881' failed
gmake[1]: *** [build-1803236881] Error 2
gmake[1]: Target 'main-build' not remade because of errors.
makefile:160: recipe for target 'all' failed
gmake: *** [all] Error 2

**** Build Finished ****

Thanks,

Ushasri.