Part Number: TMP411
Hello team,
I received 2 questions from the customer.
1. Which of the following is the value read from the local temperature and remote temperature registers when the BUSY bit is ON (1)?
Discarded as an undefined value or Previous value is retained.
The datasheet only describes the status during conversion, and I could not find any description of the status of the temperature registers.
2. After a power-on reset, I set the RANGE bit in the configuration register to 1 and am operating with extended temperature settings, but it is taking more than 10 seconds for the settings to be reflected in the local temperature. Can you tell me how to set the register? *The remote temperature is reflected immediately.
Regards,
Masa