Hi Ti, I'm testing LDC1612 and now I found a problem, when the target is in steady state, the output data of LDC1612 is not a straight line. I want to know why and how to improve my design.Help me please~~~
L:Ferrite Magnetic Can(shield)+ PCB coil
C:1000pF /np0/1%
target : 90mm*90mm steel
distance:1~3mm
config @1mm
config @3mm
Idrive settings
The target has been stationary, why is the data still rising?
Action 10μm, sampling 7000 data
@1mm the LC
@3mm the LC
my test device