This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: AWR1642 SRR max range 80 to 120

Part Number: AWR1642BOOST


Hi :

  The short distance preset is multi-mode (maximum detection range 80m and 20m), how can I change it to single mode (maximum detection range 120m)?

  • Hi,

    The detection at 120m is not robust. We recommend 80m as max range.

    It is possible to select single mode by changing the define in the header file and re-compiling the demo as follows

    labs\lab0002_short_range_radar\src\common\srr_config_consts.h

    /**! @brief The multi-mode Radar mode of operation. */
    //#define SUBFRAME_CONF_SRR_USRR                   /* Two subframes, SRR80 followed by USRR20. */
    /**! @brief The USRR only mode of operation. */
    // #define SUBFRAME_CONF_USRR                   /* One subframe USRR20. */
    /**! @brief The SRR only mode of operation. */
     #define SUBFRAME_CONF_SRR                   /* One subframe SRR80. */

    Thank you
    Cesar