This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843: AWR6843: Vital sign sensing frequency in chirp config

Part Number: AWR6843
Other Parts Discussed in Thread: AWR1642, AWR1843, IWR6843

The Occupancy & Vital Signs Detection User's Guide (User's Guide (ti.com)) features AWR6843 EVM (60GHz) and AWR1843, AWR1642 EVMs (77GHz) as HW. But the chirp configuration part of this document features only 77GHz as chirp start frequency, for both occupancy detection and vital sign sensing. Can I use AWR6843's 60GHz SDK to do both instead? I assume 60GHz related chirp configuration is available in SDK documentation right?

PS: the links on this page to demo are expired.