This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642: DSPCLK IWR1642

Part Number: IWR1642


Dear Sirs:

  Per the TRM for 16xx

p293, DSPCLK is from PLLCLK_600 which is divided from PLLCLK_1200. But I didn't see any multiplier or divider registers inside the TRM to describe.

I want to know is there any PLL divider register between PLLCLK_1200 to PLLCLK_600? Or it is always fixed to divided by 2 in H/W?

Regards,

/ckhsu