Hi,
I'm currently undertaking a project to sense human vital signs and ECG using mmwave radar. I've chosen to use AWR1843BOOST in my experiment. Since ECG sensing requires a high FPS, may I ask if AWR1843BOOST is able to achieve a FPS of 200 (or at least above 120) theoretically and practically?
I'm currently trying to write a Python script to configure the radar and receive point cloud data from UART through USB. The script is based on the MATLAB demo code. However I'm getting all zeros for z-axis and doppler velocity when I try to increase the fps. I have attached my radar configuration with mmwave_sdk_03_06_00_00-LTS. Any suggestions?
Thanks.
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 10 7 60 0 0 65 1 256 5000 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
frameCfg 0 1 16 0 5 1 0
lowPower 0 0
guiMonitor -1 1 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 15 0
cfarCfg -1 1 0 4 2 3 1 15 0
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
lvdsStreamCfg -1 0 0 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
sensorStart