Other Parts Discussed in Thread: UNIFLASH
I want to use AWR1843 as mmWave Radar.
Are there the things which have to implemented with SW in advance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi hiroyuki,
You can refer the demo application and mmwave sdk for developing drivers and the custom application.
There is no such software which needs to be implemented in advance.
Regards,
Saswat Kumar
Thank you for your replying.
I want ask two questions.
Firstly, Please tell me like the gui to flush to AWR1843 as possible as .(I think the gui is UniFlash.)
Secondly, Are there ways to confirm AWR1843 driving?
(Both please tell me your recommended way both SW and HW.)
Hello Hiroyuki,
1) Yes the uniflash is the tool that is used for flashing the AWR1843. The user guide present in the mmwave sdk is the one that provides the information on this flashing steps in section 4.2 the path is C:\ti\mmwave_sdk_03_05_00_04\docs\mmwave_sdk_user_guide.pdf
2) in the mmwave sdk we have the various examples for drivers that are present. You can run these examples and the demo to check if the board is behaving as expected. Also additionally, if there is an AWR1843 EVM present you could run the same applications and cross verify it as well.
Regards,
Saswat Kumar