This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: How to run Autonomous Robotics lab with my EVM.

Part Number: IWR1843BOOST


Hi,

I am using IWR1843BOOST EVM. Details are-

MMWave SDK-3.5 (reflashed the EVM also with mmwave_sdk-3.5 out-of-box bin file)

Industrial Toolbox - 4.12.0

ROS melodic image

Done ROS driver setup-

https://dev.ti.com/tirex/explore/node?node=ANNtaxZONu0PbSaUU.YiPQ__VLyFKFf__LATEST

Able to run the command- "roslaunch ti_mmwave_rospkg 1843_multi_3d_0.launch". EVM is also glowing the 3rd(GPIO_2) and Got output-

'''

[ INFO] [1662701520.471239496]: mmWaveQuickConfig: mmWaveQuickConfig will now terminate. Done configuring mmWave device using config file: /opt/catkin_ws/src/mmwave_ti_ros/ros_driver/src/ti_mmwave_rospkg/cfg/1843_3d.cfg
[ INFO] [1662701520.475577613]:

==============================
List of parameters
==============================
Number of range samples: 256
Number of chirps: 16
f_s: 5.209 MHz
f_c: 79.210 GHz
Bandwidth: 3440.200 MHz
PRI: 324.140 us
Frame time: 100.000 ms
Max range: 11.154 m
Range resolution: 0.044 m
Max Doppler: +-0.973 m/s
Doppler resolution: 0.122 m/s
==============================

[ INFO] [1662701520.478388885]: DataUARTHandler Read Thread: Port is open
[radar_0/ti_mmwave_config-3] process has finished cleanly
log file: /root/.ros/log/b9638002-3000-11ed-8bbf-9cfce8f48da0/radar_0-ti_mmwave_config-3*.log

'''

Issue-

Ran the RVIZ-

PointCloud2->/mmWaveDataHdl/RScan

What is the "Fixed_Frame" in Global_option ? as it is default "map" -> giving error in RVIZ. And if i change to "ti_mmwave_0" -> no error but no pointclound.

Also in rostopic list, there is no such message named "/mmWaveDataHdl/RScan".

Note-

when i changed Fixed_frame in Global_option to "ti_mmwave_pcl" -> then i can see messages are being received in PointCloud2, but error is "Failed to transform from frame [/ti_mmwave_0] to frame [ti_mmwave_pcl]"

2) 

Trying to run -

https://dev.ti.com/tirex/explore/node?node=AC04mnRRMBdrhkYsRzjrEQ__VLyFKFf__LATEST

All setup done. But still not able to get the pointcloud output.

Will this Example run without Turtlebot robot? i just want pointcloud.

Will this work with IWR1843BOOST EVM or not?

Thanks.

  • Hello,

    The ROS Driver fully supports the IWR1843BOOST EVM and you do not need a Turtlebot robot for this demo in order to get a point cloud from your EVM. Based off of your log the sensor started successfully based off of the config. Is the config file you are using simply the default one? Is the .launch file you are using unedited as well?

    RScan is an object of type RadarScan (A message) that you can find defined and used in DataHandlerClass.cpp located in the src folder. Within this file you should also be able to find the section that sends the point cloud which is within the switch case of "READ_OBJ_STRUCT". Feel free to add ROS comments here via ROS_INFO and make changes to see if that portion of code is ever reached. This should help narrow down the debug process. Make sure to do catkin_make on your project after making any changes to a .cpp file.

    Best Regards,

    Pedrhom Nafisi 

  • Hi , Thanks for the reply.

    I am able to get the Pointcloud with ROS driver. I did following-

    I changed, frame_id = /ti_mmwave_0 to frame_id = ti_mmwave_0 .

    In RVIZ, PointCloud2->(Topic) /ti_mmwave/radar_scan_pcl_0

    And pointcloud started apearing. May be TI Ros Driver is updated in term of msgs.

    2) Now proceeding further for Autonomous Robot Lab for the same "https://dev.ti.com/tirex/explore/node?node=AC04mnRRMBdrhkYsRzjrEQ__VLyFKFf__LATEST", i did all setup. But there i am not able to find the pointcloud at all.

    Any suggestion to run Autonomous Robot Lab ?

    Thanks.

  • Update-

    These are my steps-

    roslaunch turtlebot_bringup minimal_single_sensor.launch mmwave_device:=1843

    Use the following command to fix incorrect tag usage:
    find . -iname "*.xacro" | xargs sed -i 's#<\([/]\?\)\(if\|unless\|include\|arg\|property\|macro\|insert_block\)#<\1xacro:\2#g'

    started roslaunch server http://rahul-IdeaPad:44695/

    SUMMARY
    ========

    PARAMETERS
    * /bumper2pointcloud/pointcloud_radius: 0.24
    * /cmd_vel_mux/yaml_cfg_file: /opt/catkin_ws/sr...
    * /diagnostic_aggregator/analyzers/input_ports/contains: ['Digital Input',...
    * /diagnostic_aggregator/analyzers/input_ports/path: Input Ports
    * /diagnostic_aggregator/analyzers/input_ports/remove_prefix: mobile_base_nodel...
    * /diagnostic_aggregator/analyzers/input_ports/timeout: 5.0
    * /diagnostic_aggregator/analyzers/input_ports/type: diagnostic_aggreg...
    * /diagnostic_aggregator/analyzers/kobuki/contains: ['Watchdog', 'Mot...
    * /diagnostic_aggregator/analyzers/kobuki/path: Kobuki
    * /diagnostic_aggregator/analyzers/kobuki/remove_prefix: mobile_base_nodel...
    * /diagnostic_aggregator/analyzers/kobuki/timeout: 5.0
    * /diagnostic_aggregator/analyzers/kobuki/type: diagnostic_aggreg...
    * /diagnostic_aggregator/analyzers/power/contains: ['Battery', 'Lapt...
    * /diagnostic_aggregator/analyzers/power/path: Power System
    * /diagnostic_aggregator/analyzers/power/remove_prefix: mobile_base_nodel...
    * /diagnostic_aggregator/analyzers/power/timeout: 5.0
    * /diagnostic_aggregator/analyzers/power/type: diagnostic_aggreg...
    * /diagnostic_aggregator/analyzers/sensors/contains: ['Cliff Sensor', ...
    * /diagnostic_aggregator/analyzers/sensors/path: Sensors
    * /diagnostic_aggregator/analyzers/sensors/remove_prefix: mobile_base_nodel...
    * /diagnostic_aggregator/analyzers/sensors/timeout: 5.0
    * /diagnostic_aggregator/analyzers/sensors/type: diagnostic_aggreg...
    * /diagnostic_aggregator/base_path:
    * /diagnostic_aggregator/pub_rate: 1.0
    * /mobile_base/base_frame: base_footprint
    * /mobile_base/battery_capacity: 16.5
    * /mobile_base/battery_dangerous: 13.2
    * /mobile_base/battery_low: 14.0
    * /mobile_base/cmd_vel_timeout: 0.6
    * /mobile_base/device_port: /dev/kobuki
    * /mobile_base/odom_frame: odom
    * /mobile_base/publish_tf: True
    * /mobile_base/use_imu_heading: True
    * /mobile_base/wheel_left_joint_name: wheel_left_joint
    * /mobile_base/wheel_right_joint_name: wheel_right_joint
    * /radar_0/ti_mmwave/command_port: /dev/ttyACM0
    * /radar_0/ti_mmwave/command_rate: 115200
    * /radar_0/ti_mmwave/data_port: /dev/ttyACM1
    * /radar_0/ti_mmwave/data_rate: 921600
    * /radar_0/ti_mmwave/frame_id: ti_mmwave
    * /radar_0/ti_mmwave/max_allowed_azimuth_angle_deg: 60
    * /radar_0/ti_mmwave/max_allowed_elevation_angle_deg: 30
    * /radar_0/ti_mmwave/mmWaveCLI_name: /mmWaveCLI
    * /radar_0/ti_mmwave_config/mmWaveCLI_name: /mmWaveCLI
    * /robot/name: turtlebot
    * /robot/type: turtlebot
    * /robot_description: <?xml version="1....
    * /robot_state_publisher/publish_frequency: 5.0
    * /rosdistro: melodic
    * /rosversion: 1.14.13
    * /use_sim_time: False

    NODES
    /
    bumper2pointcloud (nodelet/nodelet)
    cmd_vel_mux (nodelet/nodelet)
    diagnostic_aggregator (diagnostic_aggregator/aggregator_node)
    hector_trajectory_server (hector_trajectory_server/hector_trajectory_server)
    mobile_base (nodelet/nodelet)
    mobile_base_nodelet_manager (nodelet/nodelet)
    radar_baselink_0 (tf/static_transform_publisher)
    robot_state_publisher (robot_state_publisher/robot_state_publisher)
    rviz (rviz/rviz)
    tf_base_link_to_base_footprint (tf/static_transform_publisher)
    /radar_0/
    ti_mmwave (ti_mmwave_rospkg/ti_mmwave_rospkg)
    ti_mmwave_config (ti_mmwave_rospkg/mmWaveQuickConfig)

    auto-starting new master
    process[master]: started with pid [193758]
    ROS_MASTER_URI=http://localhost:11311

    setting /run_id to 7f565c36-326c-11ed-9dcd-9cfce8f48da0
    process[rosout-1]: started with pid [193769]
    started core service [/rosout]
    process[robot_state_publisher-2]: started with pid [193776]
    process[diagnostic_aggregator-3]: started with pid [193777]
    process[radar_0/ti_mmwave-4]: started with pid [193784]
    [ INFO] [1662967711.633030088]: Initializing nodelet with 8 worker threads.
    [ INFO] [1662967711.642742182]: mmWaveCommSrv: command_port = /dev/ttyACM0
    [ INFO] [1662967711.642816060]: mmWaveCommSrv: command_rate = 115200
    [ INFO] [1662967711.647783334]: mmWaveDataHdl: data_port = /dev/ttyACM1
    [ INFO] [1662967711.647839038]: mmWaveDataHdl: data_rate = 921600
    [ INFO] [1662967711.647861250]: mmWaveDataHdl: max_allowed_elevation_angle_deg = 30
    [ INFO] [1662967711.647882118]: mmWaveDataHdl: max_allowed_azimuth_angle_deg = 60
    process[radar_0/ti_mmwave_config-5]: started with pid [193790]
    [ INFO] [1662967711.710032020]: mmWaveQuickConfig: Configuring mmWave device using config file: /opt/catkin_ws/src/mmwave_ti_ros/autonomous_robotics_ros/src/ti_mmwave_rospkg/cfg/1843_3d.cfg
    process[radar_baselink_0-6]: started with pid [193806]
    process[rviz-7]: started with pid [193812]
    QStandardPaths: XDG_RUNTIME_DIR not set, defaulting to '/tmp/runtime-root'
    process[hector_trajectory_server-8]: started with pid [193818]
    process[tf_base_link_to_base_footprint-9]: started with pid [193825]
    [ INFO] [1662967712.223623755]: mmWaveCommSrv: Sending command to sensor: 'sensorStop'
    [ INFO] [1662967712.229797158]: mmWaveCommSrv: Received response from sensor: 'sensorStop
    Ignored: Sensor is already stopped
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.233332882]: mmWaveCommSrv: Sending command to sensor: 'flushCfg'
    [ INFO] [1662967712.236043207]: mmWaveCommSrv: Received response from sensor: 'flushCfg
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.239766371]: mmWaveCommSrv: Sending command to sensor: 'dfeDataOutputMode 1'
    [ INFO] [1662967712.243768865]: mmWaveCommSrv: Received response from sensor: 'dfeDataOutputMode 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.247425675]: mmWaveCommSrv: Sending command to sensor: 'channelCfg 15 7 0'
    [ INFO] [1662967712.250976748]: mmWaveCommSrv: Received response from sensor: 'channelCfg 15 7 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.254346854]: mmWaveCommSrv: Sending command to sensor: 'adcCfg 2 1'
    process[mobile_base_nodelet_manager-10]: started with pid [193864]
    [ INFO] [1662967712.257689799]: mmWaveCommSrv: Received response from sensor: 'adcCfg 2 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.268985105]: mmWaveCommSrv: Sending command to sensor: 'adcbufCfg -1 0 1 1 1'
    [ INFO] [1662967712.272763922]: mmWaveCommSrv: Received response from sensor: 'adcbufCfg -1 0 1 1 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.275928224]: mmWaveCommSrv: Sending command to sensor: 'profileCfg 0 77 267 7 57.14 0 0 70 1 256 5209 0 0 30'
    [ INFO] [1662967712.282506582]: mmWaveCommSrv: Received response from sensor: 'profileCfg 0 77 267 7 57.14 0 0 70 1 256 5209 0 0 30
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.293797771]: mmWaveCommSrv: Sending command to sensor: 'chirpCfg 0 0 0 0 0 0 0 1'
    [ INFO] [1662967712.297950396]: mmWaveCommSrv: Received response from sensor: 'chirpCfg 0 0 0 0 0 0 0 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.301371546]: mmWaveCommSrv: Sending command to sensor: 'chirpCfg 1 1 0 0 0 0 0 4'
    [ INFO] [1662967712.305555990]: mmWaveCommSrv: Received response from sensor: 'chirpCfg 1 1 0 0 0 0 0 4
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.360133199]: mmWaveCommSrv: Sending command to sensor: 'chirpCfg 2 2 0 0 0 0 0 2'
    [ INFO] [1662967712.364573590]: mmWaveCommSrv: Received response from sensor: 'chirpCfg 2 2 0 0 0 0 0 2
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.368999304]: mmWaveCommSrv: Sending command to sensor: 'frameCfg 0 2 16 0 100 1 0'
    [ INFO] [1662967712.373392267]: mmWaveCommSrv: Received response from sensor: 'frameCfg 0 2 16 0 100 1 0
    Done
    mmwDemo:/>'
    process[mobile_base-11]: started with pid [193871]
    [ INFO] [1662967712.382615679]: mmWaveCommSrv: Sending command to sensor: 'lowPower 0 0'
    [ INFO] [1662967712.386106369]: mmWaveCommSrv: Received response from sensor: 'lowPower 0 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.390766500]: mmWaveCommSrv: Sending command to sensor: 'guiMonitor -1 1 1 0 0 0 1'
    [ INFO] [1662967712.396041699]: mmWaveCommSrv: Received response from sensor: 'guiMonitor -1 1 1 0 0 0 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.398585473]: mmWaveCommSrv: Sending command to sensor: 'cfarCfg -1 0 2 8 4 3 0 15 1'
    [ INFO] [1662967712.402979679]: mmWaveCommSrv: Received response from sensor: 'cfarCfg -1 0 2 8 4 3 0 15 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.406426246]: mmWaveCommSrv: Sending command to sensor: 'cfarCfg -1 1 0 4 2 3 1 15 1'
    [ INFO] [1662967712.410873020]: mmWaveCommSrv: Received response from sensor: 'cfarCfg -1 1 0 4 2 3 1 15 1
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.420978336]: mmWaveCommSrv: Sending command to sensor: 'multiObjBeamForming -1 1 0.5'
    [ INFO] [1662967712.425502454]: mmWaveCommSrv: Received response from sensor: 'multiObjBeamForming -1 1 0.5
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.432908757]: mmWaveCommSrv: Sending command to sensor: 'clutterRemoval -1 0'
    [ INFO] [1662967712.436615019]: mmWaveCommSrv: Received response from sensor: 'clutterRemoval -1 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.441968924]: mmWaveCommSrv: Sending command to sensor: 'calibDcRangeSig -1 0 -5 8 256'
    [ INFO] [1662967712.446632161]: mmWaveCommSrv: Received response from sensor: 'calibDcRangeSig -1 0 -5 8 256
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.451511061]: mmWaveCommSrv: Sending command to sensor: 'extendedMaxVelocity -1 0'
    [ INFO] [1662967712.455664898]: mmWaveCommSrv: Received response from sensor: 'extendedMaxVelocity -1 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.468390422]: mmWaveCommSrv: Sending command to sensor: 'lvdsStreamCfg -1 0 0 0'
    [ INFO] [1662967712.472358632]: mmWaveCommSrv: Received response from sensor: 'lvdsStreamCfg -1 0 0 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.476305002]: mmWaveCommSrv: Sending command to sensor: 'compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0'
    process[bumper2pointcloud-12]: started with pid [193898]
    [ INFO] [1662967712.485448986]: mmWaveCommSrv: Received response from sensor: 'compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.491311650]: mmWaveCommSrv: Sending command to sensor: 'measureRangeBiasAndRxChanPhase 0 1.5 0.2'
    [ INFO] [1662967712.496872821]: mmWaveCommSrv: Received response from sensor: 'measureRangeBiasAndRxChanPhase 0 1.5 0.2
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.508698677]: mmWaveCommSrv: Sending command to sensor: 'CQRxSatMonitor 0 3 5 121 0'
    [ INFO] [1662967712.513062466]: mmWaveCommSrv: Received response from sensor: 'CQRxSatMonitor 0 3 5 121 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.517363678]: mmWaveCommSrv: Sending command to sensor: 'CQSigImgMonitor 0 127 4'
    [ INFO] [1662967712.521282837]: mmWaveCommSrv: Received response from sensor: 'CQSigImgMonitor 0 127 4
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.525856066]: mmWaveCommSrv: Sending command to sensor: 'analogMonitor 0 0'
    [ INFO] [1662967712.529366894]: mmWaveCommSrv: Received response from sensor: 'analogMonitor 0 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.533987192]: mmWaveCommSrv: Sending command to sensor: 'aoaFovCfg -1 -90 90 -90 90'
    [ INFO] [1662967712.538300877]: mmWaveCommSrv: Received response from sensor: 'aoaFovCfg -1 -90 90 -90 90
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.542898992]: mmWaveCommSrv: Sending command to sensor: 'cfarFovCfg -1 0 0 8.92'
    [ INFO] [1662967712.546873364]: mmWaveCommSrv: Received response from sensor: 'cfarFovCfg -1 0 0 8.92
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.551153737]: mmWaveCommSrv: Sending command to sensor: 'cfarFovCfg -1 1 -1 1.00'
    [ INFO] [1662967712.554976707]: mmWaveCommSrv: Received response from sensor: 'cfarFovCfg -1 1 -1 1.00
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.559404264]: mmWaveCommSrv: Sending command to sensor: 'calibData 0 0 0'
    [ INFO] [1662967712.562502753]: mmWaveCommSrv: Received response from sensor: 'calibData 0 0 0
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.566082931]: mmWaveCommSrv: Sending command to sensor: 'sensorStart'
    [ WARN] [1662967712.585577258]: Kobuki : device does not (yet) available, is the usb connected?.
    process[cmd_vel_mux-13]: started with pid [193904]
    [ INFO] [1662967712.674608925]: mmWaveCommSrv: Received response from sensor: 'sensorStart
    Debug: Init Calibration Status = 0x1ffe
    Done
    mmwDemo:/>'
    [ INFO] [1662967712.695917586]: mmWaveQuickConfig: mmWaveQuickConfig will now terminate. Done configuring mmWave device using config file: /opt/catkin_ws/src/mmwave_ti_ros/autonomous_robotics_ros/src/ti_mmwave_rospkg/cfg/1843_3d.cfg
    [ INFO] [1662967712.699735326]:

    ==============================
    List of parameters
    ==============================
    Number of range samples: 256
    Number of chirps: 16
    f_s: 5.209 MHz
    f_c: 79.210 GHz
    Bandwidth: 3440.200 MHz
    PRI: 324.140 us
    Frame time: 100.000 ms
    Max range: 11.154 m
    Range resolution: 0.044 m
    Max Doppler: +-0.973 m/s
    Doppler resolution: 0.122 m/s
    ==============================

    [ INFO] [1662967712.701612567]: DataUARTHandler Read Thread: Port is open
    [ WARN] [1662967712.836108316]: Kobuki : no data stream, is kobuki turned on?
    [radar_0/ti_mmwave_config-5] process has finished cleanly
    log file: /root/.ros/log/7f565c36-326c-11ed-9dcd-9cfce8f48da0/radar_0-ti_mmwave_config-5*.log
    [ WARN] [1662967732.077381458]: No transform between frames map and base_link available after 20.004478 seconds of waiting. This warning only prints once.
    QObject::connect: Cannot queue arguments of type 'QVector<int>'
    (Make sure 'QVector<int>' is registered using qRegisterMetaType().)
    QObject::connect: Cannot queue arguments of type 'QVector<int>'
    (Make sure 'QVector<int>' is registered using qRegisterMetaType().)


    Then running "roslaunch turtlebot_mmwave_launchers radar_mapping.launch"-

    i am getting output-

    process[static_tf_map_to_odom-1]: started with pid [177280]
    process[pcl_manager-2]: started with pid [177281]
    [ INFO] [1662966523.376216954]: Initializing nodelet with 8 worker threads.
    process[x_filt-3]: started with pid [177287]
    [ INFO] [1662966523.454497339]: Loading nodelet /x_filt of type pcl/PassThrough to manager pcl_manager with the following remappings:
    [ INFO] [1662966523.455543838]: /x_filt/input -> /ti_mmwave/radar_scan_pcl
    [ INFO] [1662966523.455559097]: /x_filt/output -> /x_filt_out
    process[y_filt-4]: started with pid [177303]
    [ INFO] [1662966523.593627710]: Loading nodelet /y_filt of type pcl/PassThrough to manager pcl_manager with the following remappings:
    [ INFO] [1662966523.594699928]: /y_filt/input -> /x_filt_out
    [ INFO] [1662966523.594720096]: /y_filt/output -> /xy_filt_out
    process[z_filt-5]: started with pid [177316]
    [ INFO] [1662966523.712346442]: Loading nodelet /z_filt of type pcl/PassThrough to manager pcl_manager with the following remappings:
    [ INFO] [1662966523.713679791]: /z_filt/input -> /xy_filt_out
    [ INFO] [1662966523.713713724]: /z_filt/output -> /xyz_filt_out
    process[i_filt-6]: started with pid [177321]
    [ INFO] [1662966523.829475531]: Loading nodelet /i_filt of type pcl/PassThrough to manager pcl_manager with the following remappings:
    [ INFO] [1662966523.830572185]: /i_filt/input -> /xyz_filt_out
    [ INFO] [1662966523.830599236]: /i_filt/output -> /xyzi_filt_out
    process[octomap_raw-7]: started with pid [177330]
    process[mapping_SOR_filt_mapping-8]: started with pid [177339]
    [ INFO] [1662966524.091831761]: Publishing latched (single publish will take longer, all topics are prepared)
    type is pcl/StatisticalOutlierRemoval
    [ WARN] [1662966524.113734848]: Nothing to publish, octree is empty
    process[octomap_filtered-9]: started with pid [177348]
    [ INFO] [1662966524.360708566]: Publishing latched (single publish will take longer, all topics are prepared)
    [ WARN] [1662966524.376596042]: Nothing to publish, octree is empty
    Warning: TF_OLD_DATA ignoring data from the past for frame base_link at time 1.66297e+09 according to authority unknown_publisher
    Possible reasons are listed at wiki.ros.org/.../Errors explained
    at line 277 in /tmp/binarydeb/ros-melodic-tf2-0.6.5/src/buffer_core.cpp
    [ WARN] [1662966539.129692982]: MessageFilter [target=/map ]: Dropped 100.00% of messages so far. Please turn the [ros.octomap_server.message_filter] rosconsole logger to DEBUG for more information.
    [ WARN] [1662966599.139789726]: MessageFilter [target=/map ]: Dropped 100.00% of messages so far. Please turn the [ros.octomap_server.message_filter] rosconsole logger to DEBUG for more information.
    [ WARN] [1662966659.149641836]: MessageFilter [target=/map ]: Dropped 100.00% of messages so far. Please turn the [ros.octomap_server.message_filter] rosconsole logger to DEBUG for more information.

    [ WARN] [1662968214.817407306]: MessageFilter [target=/map ]: Dropped 100.00% of messages so far. Please turn the [ros.octomap_server.message_filter] rosconsole logger to DEBUG for more information.
    [ WARN] [1662968274.827425636]: MessageFilter [target=/map ]: Dropped 100.00% of messages so far. Please turn the [ros.octomap_server.message_filter] rosconsole logger to DEBUG for more information.

    Also in RVIZ, there is error for "RobotModel" -

    Why i am not able to generate the map?

    If i put Global_fixed_frame -> base_link, and PointCloud->/ti_mmwave/radar_scan_pcl, then raw pointclouds are there. But

    If i put Global_fixed_frame -> map, then there is no pointcloud with PointCloud->/ti_mmwave/radar_scan_pcl, or PointCloud->/filtered_point_cloud_centers

    Attached screenshots are for reference-

    Please suggest how can i do mapping demo run....?

  • Hello,

    Unfortunately the Autonomous Robot Lab requires specifically a Kobuki based TurtleBot platform in order to work, and is why you are getting messages about no Kobuki being detected. http://kobuki.yujinrobot.com/about2/

    There is also an error for RobotModel as none was detected based on your setup. Using "roslaunch turtlebot_mmwave_launchers radar_navigation_single.launch" you will at least be using the correct launch file to load the model and the launch file used in this demo, but ultimately without a TurtleBot you cannot run this demo. Below is a list of all the packages used and all the ones bolded require a platform such as Kobuki.

    bumper2pointcloud (nodelet/nodelet)
    cmd_vel_mux (nodelet/nodelet)
    diagnostic_aggregator (diagnostic_aggregator/aggregator_node)
    hector_trajectory_server (hector_trajectory_server/hector_trajectory_server)
    mobile_base (nodelet/nodelet)
    mobile_base_nodelet_manager (nodelet/nodelet)
    radar_baselink_0 (tf/static_transform_publisher)
    robot_state_publisher (robot_state_publisher/robot_state_publisher)
    rviz (rviz/rviz)
    tf_base_link_to_base_footprint (tf/static_transform_publisher)
    /radar_0/
    ti_mmwave (ti_mmwave_rospkg/ti_mmwave_rospkg)
    ti_mmwave_config (ti_mmwave_rospkg/mmWaveQuickConfig)

    With only the sensor the furthest you can go without your own independent development is what is provided with the ROS Driver that gives the PointCloud information. As suggested prior, I recommend you look at DataHandlerClass.cpp as that is where the data is pulled in from the sensor, what you want to do with that data afterwards is all up to you.

    Best Regards,

    Pedrhom Nafisi