This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5170UEVM: TMAG5170EVM Sensor dimensions/CAD Model (Width of Board+Sensor)

Part Number: TMAG5170UEVM


Hello,

I see in other comments there are dimensions of the board given, but I cannot find the width of the PCB at the location of the sensor. Are there more detailed drawings or preferable a CAD model available?

Thanks,

Thomas

  • Thomas,

    Here's a STEP file of the PCB

    Thanks,

    Scott

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/SENS083A.step

  • Hello Thomas,

    Thanks for posting to the sensing forum! The complete PCB is about 27.325mm x 45.72mm unsnapped, if you snap it and remove one of the sensors then you are looking at 27.325mm x 22.86mm. The information about the sensor package itself should be on the datasheet and CAD files should be available for the sensor itself in the product page, ou can click on design and development: https://www.ti.com/product/TMAG5170

    For the EVM I was able to generate a step file for you but it is of the two boards together, I hope this works!

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/SENS083.step

    Best,

    Isaac