Other Parts Discussed in Thread: IWR1843BOOST
Hello,
My customer has evaluated the MRR lab from the Automotive Toolbox v3.6. Detection works fine up to 140 meters, but they have an issue with the tracker id consistency which does not seem to be kept during the target's trajectory.
They have then evaluated the beam steering lab from the same toolbox in an almost identical setting. The issue is the detection is much poorer, up to meters only.
Could you please advise on how to solve that? One thought would be to integrate Gtrack into MRR, but before going there, we are wondering whether there is any reason for the beam steering MRR to be less performant than MRR.
The setup differences are the following:
Lab | MRR | Beam steering MRR |
Sub-frames used | MRR | USRR+MRR |
Steering angle | n/a | -40 to +40°, 20° increment |
Thank you.
Best regards,
François.