Other Parts Discussed in Thread: IWR6843, IWR6843AOP
I want to implement an Advanced Frame Configuration which contains 2 or more chirps with different Frequency ramp values and different ADC start times.
The mmwave SDK version 3.6 contains a config file with a similar requirement, at the location <mmwave SDK>\packages\ti\demo\xwr68xx\mmw\profiles\profile_advanced_subframe.cfg. Is there any lab that supports this profile?
I tried to use this demo file with both the Demo visualizer and the C code provided by TI. While using the above mention chirp profile with the Demo visualizer I get an error saying bpmCfg is not supported which makes sense as the cliCfg.tableEntry[cnt].cmd code doesn't contain the bpmCfg command.
I saw an implementation of the Advanced Frame config with 4 different chirps in a frame in Long range people detection lab, their frequency ramp parameters were the same but the transmit power backoff parameter was different. It contains an implementation of the bpmCFg command as well.
How can I implement the bpmCfg parser, as in what would be right way to include the bpmCfg dependent functions from Long range people detection lab to Out of the box demo lab?
What are the steps to implement an Advanced frame in my application?
Also, OOB lab C code for 6843 ODS is implemented on MSS only. What steps should I follow to use DSS as well?