Does mmWave API contain all of function of mmWave Link?
(I think mmWave API is wrapper for mmWave link. Like the below figure.)
(p.s.)
Are there any functions that cannot be done with the mmWave API but can be done with the mmWave Link?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does mmWave API contain all of function of mmWave Link?
(I think mmWave API is wrapper for mmWave link. Like the below figure.)
(p.s.)
Are there any functions that cannot be done with the mmWave API but can be done with the mmWave Link?
Hi,
The mmWave Link provides low level API's to control, configure and monitor the RF sub system. mmWave API's is a more abstracted version of mmWave Link which is more convenient and easier to use for users. It in turn uses all the API's from mmWave Link. If your application requires more control/ you want to use more complex features of the RF subsystem then you can use the Link API's. It will depend on your application requirement.
Thanks,
Pradipta.