This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: AWR2243's SPI function MOSI pin should set pull up or pull down resistor?

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: AWR2243

In AWR2243 datasheet, SPI function MOSI pin's default pull status is pull up,

But in 《PROC054E_AWR_Pull_Resistors.SchDoc》,this pin has a pull down resistor.

There are different, which one is correct ?

  • Hi,

         I think you are referring to two different things. The DS talks about status of PULL structures associated with the IO after device POWER UP. Where as the Board schematic is talking about the external recommended interface. This signal is also going to the HOST.

    Regards