Greeting,
I am currently following the mm studio cascade user guide at 19 page, 7.3.3 capture data.
I have met the problem that no files have been captured in the SSD directory.
1. Click on TDAxxArm with Radar device 1.
2. Folder is created under /mnt/ssd directory in TDA2XX
3. Click on Trigger frame for all the enable slave devices.
4. Farming status is WAITING FOR TRIGGER.
mmWaveStudio view
5. Click on Trigger frame for Master (Radar device 1).
6. Framing status is FRAMING for an instant.
7. No files have been captured in created folder.
Win SCP view
Best regards