This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC6821-Q1: How to connect IN+/IN- if we do not need remote temperature sensing

Part Number: AMC6821-Q1
Other Parts Discussed in Thread: AMC6821

Hi team,

I would like to confirm with you one question below.

  • How to connect IN+/IN- if we do not need remote temperature sensing?

Thanks.

Johnny

  • Hi Johnny,

    AMC6821 will operate without a remote junction, but many features will not be available. The IN pins can be left floating. Page 16, under the heading Remote Temperature Sensor Failure Detection describes that the AMC6821 will report -128C as the remote temperature. The RTF bit will also be set, and the SMBALERT will be triggered on every conversion. I would recommend connecting a small MMBT3904 or similar near the AMC6821 instead.

    thanks,

    ren