This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Disposal of unused pins

Part Number: AWR1843

I used AWR1843
I am designing a circuit.
If you do not wire the following pins, this pin is
Is there any problem with opening?

R4,P4,R5,P5,P6,R7,P7,R8,P8,N15,N14,M15,M14,L15,L14,K15,K14,J15,J14,H14,H13,E14,E13,D14,D13, C13