This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: Can I send the phrase information from one mmWave radar to another one?

Part Number: IWR1843

Hi,

Suppose I have two radars: one is the Sender, another is the Receiver.  I want to send the phrase \alpha from the Sender to the Receiver.

Firstly, I construct two signals in the Sender, difference of their phrases is \alpha, and send these two signals one by one. (I find TI's radar has the phrase shifter configuration api, so I think it is possible)

Then, the Receiver gets these two signals, and compute the \alpha by comparing them.

Can I achieve the above function using two TI's mmWave radars. Thanks.