Other Parts Discussed in Thread: HDC2021, HDC1080, HDC2080, HDC2022
Do we have suitable solution can replace SI7021-A20-GM.
Thanks a lot!
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Thank you for posting to the Sensing forum!
If you want P2P compatible parts, the HDC2080, HDC2021, HDC2022 and the HDC1080 are great options. The HDC2 options allows users to configure the devices with 2 different I2C addresses. The type of device would depend on the application, accuracy and if you need a filter or a protective cover or not.
If you want a higher accuracy device, you can also check out the HDC3 family. However, these devices are not P2P compatible.
Regards,
Pavani Tenenti