This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST-ODS: AWR1642BOOST code compatibility with AWR1642-ODS EVM

Genius 11600 points
Part Number: AWR1642BOOST-ODS
Other Parts Discussed in Thread: AWR1642BOOST

Dear team,

I just got my AWR1642BOOST and was looking at Automotive Toolbox (3.6.0). I noticed that there is an "Obstacle Detection" lab for AWR1642-ODS EVM. I want to try it out, would sample codes intended for AWR1642-ODS EVM work on AWR1642BOOST?

And can I use AWR1642BOOST for obstacle detection purposes, I saw ODS model after I received Boost so I am quite curious..

Thanks in advance


Best Regards,
William

  • Hi,

    The demo designed for ODS evm will not run with boost evm

    We recommend using the mmWave SDK demo for boost evm. It will provide good performance as well for obstacle detection

    The only advantage of the ods EVM is that it provides

    • larger FOV
    • higher angular resolution for elevation

    Thank you

    Cesar