Other Parts Discussed in Thread: IWR1843,
For chirps from one radar to another, "It is not possible to transmit chirps from the IWR1843 to be received by the IWR1443. This is because in order for the radar to process a received signal, it needs to be mixed with the original transmit signal, but since the board is only receiving, it has no reference point to demodulate the received signal. "
So If we can generate the same signal in two different radars, then we can perform the mix operation. So the point is whether we can generate the same signal in different radars. Can TI's radar support is?