This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: absolute positioning: use a differential 2 channel construction

Part Number: LDC1612

Datasheet LDC1612, chapter 8.2.1 (page 49): For absolute positioning needs, it is recommended to use a differential 2 channel construction.

I didn't found further explanations about this. Where can I get more information about ABSOLUTE positioning with LDC1612??

  • I'm not exactly sure what the original author meant by that statement, and I don't know of any additional information on that topic.

    A single channel can detect a change in linear, one-dimensional position.
    I'm guessing what the author meant was that you would need a two-channel system to detect a change in two-dimensional  {x,y} position.

    I'm emphasizing change in position because inductive sensors like the LDC1612 are better at that, compared to detecting a target's stationary position.

    You can sometimes use LDCs to detect stationary position, but it is dependent on the application & requirements.
    It also requires an up-front calibration. An example of this is the 1-Degree Dial Reference Design cited just above the sentence you mentioned.
    Note that calibration may need to be repeated if system parameters drift over time.

    Regards,
    John