This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Rev G schematic

Part Number: IWR6843AOPEVM

Hi Team,

Good day! Could you please help to check our customer's concern below.

I am testing the IWR6843AOPEVM.

I can use it with the demo application (Demo visualizer) through USB and I would like to receive the data (once the configuration is started) with another serial. basically, I want to remove the USB and use the 2 serials, but I am struggling with the S1/S2 configuration and, most important, I cannot see any serial raw data. it is supposed to be on the MSS_LOGGER pin, right?

FYI, right now I am connecting on the 60pin-connector and MSS_LOGGER should be pin 18. Unfortunately, I cannot see any data. I have rev. G hardware, but I am using rev F as reference.

So, I am testing the IWR6843AOPEVM (hw rev. G) and I want to read raw data from serial.

Raw data should be on MSS_LOGGER pin, which is directly connected to the 60-pin connector - pin18, I guess because I can see the raw stream on pin20 of the CP2105, but I cannot see the stream on the 60pin connector.

I have a quick question: where can I find the rev G schematic for the IRW6843AOPEVM board? I have the rev F (found on website) but the rev G is missing.

Best regards,

Jonathan