This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Update over CLI

Part Number: IWR6843AOP


Hi,

We are using the Mistral_60GHz-Industrial-AoP-Radar-1 device for development and evaluation.

We know that we can update the device over the UART by putting the operation/flash switch of the device in the correct position.

Is it possible to set the device in FLASH mode by means of software (preferably CLI)?
In our test setup, we like to update the device over the UART connection.

  • Hi,

    Firstly, it is beyond the scope of these forums for us to discuss what is/is not possible with a third party's hardware kit. To focus on the device level, it is possible to update the image via UART using our Secondary Bootloader (SBL). The software and example of how to do this can be found in the mmWave SDK at the following location:
    <mmWave_SDK_intall>/packages/ti/utils/sbl

    Best Regards,
    Alec