Hi technical support,
Would like to achieve an average power consumption of 10mW or less by intermittent operation in which Active (RADAR operation) and Deep Standby is repeated. The image of intermittent operation is illustrated in below diagram. (Rough idea: chirp cycle time 120us, 3fps)
1-1. Is such control possible by API?
(The image of the state is that "the lowest consumption possible while still retaining power to the device" which is described in 4.3.2.2 Full Power Down Scheme of Application Note xWR6843 Power Optimization (swra689). )
1-2. How much power consumption would be achieved by the lowest power consumption state?
1-3. What API/Command are to be used for transition to the lowest power consumption state?
2. Instead of using the above mentioned API/command, if RESET state is applied to achieve the lowest power consumption sate,
How much power consumption would be achieved during RESET state?
Best Regards,
Katsuhiro