Hi Team,
question 1
In the project verification stage, my customer will conduct optical related tests on the ALS Sensor, mainly including the response value of the ALS Sensor under different ambient light brightness, and the response value of the ALS under different illumination angles of the light source, as shown in the figure below.
Can you help provide specific test equipment information (light source model, how to place the sample, etc.) for benchmarking testing.
question 2
Since there will be a protective cover on the sensor after the actual installation, my customer needs to calibrate the ALS Sensor. Do we have any equipment for calibration? If so, please provide the corresponding equipment information (such as light source type, brightness range, etc.).