This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944: AWR2944 spectrum spread clock SSC

Part Number: AWR2944

Hi Experts

From the TRM of AWR2944, I see that SSC is supported by AWR2944, we could use this feature for EMI mitigation.

My questions are as follows:

(1) Does SSC have any side effect when enabled?  will it affect the RF performance?

(2) Which PLL SSC should be enabled to mitigate 1.6GHz spur? If there is no side effect, maybe we could enable SSC in all PLLs.

Thanks 

Ken 

  • Hello Ken,

    Yes, SSC could be used to mitigate spurs caused by the clock generated by a particular ADPLL. If you spread the Core ADPLL clock, that clock is also used to generate the frame timing of the front end. So the frame timing would also be dithered with Core ADPLL SSC. If you are using clocks from other ADPLLs for any of the interfaces, spreading those clocks would dither the interface clocks as well.

    In general, we dont recommend enablling SSC by default, use it only if you are seeing an emission issue. Are you seeing a 1.6Ghz emission failure on 2944 ? That is not expected.

    regards,

    Vivek